2021-11-04 03:53 AM
Hi,
i currently trying to interact via shellscript and stm32cubeprog cli with my stm32mp157 board.
I can run and load tfa and than uboot. But when i want to read otp, my operations get stuck.
What is the correct call for this?
In my Script is use the following :
.../STM32_Programmer_CLI --connect port=usb1 -tm 20000 serial --verbosity 1 -tm 5000 --write ./tfa_und_uboot_slow.tsv --go 0x03 -otp displ
This is my TSV:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 ./tf-a-slow-usb.stm32
- 0x03 ssbl-boot Binary none 0x0 ./uboot-slow-usb.stm32
${PROGRAMMER_BINARY} --write ./tfa_und_uboot_slow.tsv --go 0x03 -otp displ
This is the output:
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
Warning: Timeout is forced to 5000 ms
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0046002A3139510B38313636
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MP1
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-slow-usb.stm32
File : tf-a-slow-usb.stm32
Size : 213310 Bytes
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.375
RUNNING Program ...
PartID: :0x01
Error: an error occured while setting virtual partition 0xF1 alternate setting
Error: Start operation failed at partition 0x01
Error: TSV flashing service failed
RUNNING Program ...
Address: : 0x3
Error: Start operation failed
Error: Connection to target must be established before performing any OTP command.
Many thanks for any hints 🙂
2021-11-05 01:40 AM
Hi,
please try:
.../STM32_Programmer_CLI -c port=usb1 -w ./tfa_und_uboot_slow.tsv -otp displ
Works with a similar command line on my STM32MP157F-DK2 board with a simple '2 binaries' TSV file as yours.
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-dk2-usb.stm32
- 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-dk2-trusted.bin
Ensure your board is in DFU mode (empty flash or BOOT pins=0b000).
If issues, please check board UART console log.
Are you sure that your TF-A and uBoot are working ?
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2021-11-09 02:46 AM
Hi Patrick,
i tried, but no i get stucked in the TF-A:
Now i get the following Message:
WARNING: VDD unknown
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
ERROR: Boot interface 6 not supported
PANIC at PC : 0x2ffca199
Exception mode=0x00000016 at: 0x2ffca199
2021-11-10 06:53 AM
Also some tries later i get into uboot ( when i connect on UART4 )
There is following message:
RUNNING Program ...
PartID: :0x03
Reconnecting the device ...
On the console:
scanning usb for storage devices... 0 Storage Device(s) found
partitions : done
Phase=END
DFU alt info setting: done
2021-11-22 08:17 AM
Hi,
I think your TF-A and uBoot are not correctly setup regarding your custom HW.
May I suggest to look at following articles:
https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board
https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure
https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide
note that if you use CubeProgrammer with UART instead of USB, you should also use a different TF-A binary than for USB (ending with ...uart.stm32 instead of ...usb.stm32).
See https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Using_STM32Programmer_over_UART
Regards.