2021-12-16 1:57 AM
10:55:25 : ST-LINK SN : 0034003E3137510339383538
10:55:25 : ST-LINK FW : V3J8M3B5S1
10:55:25 : Board : STLINK-V3MODS
10:55:25 : Voltage : 3.29V
10:55:25 : SWD freq : 8000 KHz
10:55:25 : Connect mode: Under Reset
10:55:25 : Reset mode : Software reset
10:55:25 : Device ID : 0x429
10:55:25 : Revision ID : Rev Y
10:55:25 : UPLOADING OPTION BYTES DATA ...
10:55:25 : Bank : 0x00
10:55:25 : Address : 0x40023c1c
10:55:25 : Size : 136 Bytes
10:55:25 : Bank : 0x01
10:55:25 : Address : 0x1ff80000
10:55:25 : Size : 136 Bytes
10:55:25 : UPLOADING ...
10:55:25 : Size : 1024 Bytes
10:55:25 : Address : 0x8000000
10:55:25 : Read progress:
10:55:25 : Data read successfully
10:55:25 : Time elapsed during the read operation is: 00:00:00.003
10:55:51 : Option byte command : -ob RDP=187
10:55:51 : PROGRAMMING OPTION BYTES AREA ...
10:55:51 : Bank : 0x01
10:55:51 : Address : 0x1ff80000
10:55:51 : Size : 136 Bytes
10:55:51 : Reconnecting...
10:55:52 : Reconnected !
10:55:52 : UPLOADING OPTION BYTES DATA ...
10:55:52 : Bank : 0x00
10:55:52 : Address : 0x40023c1c
10:55:52 : Size : 136 Bytes
10:55:52 : Bank : 0x01
10:55:52 : Address : 0x1ff80000
10:55:52 : Size : 136 Bytes
10:55:52 : OPTION BYTE PROGRAMMING VERIFICATION:
10:55:52 : Error: Expected value for Option Byte "RDP": 0xBB, found: 0xAA
10:55:52 : Error: Option Byte Programming failed
Solved! Go to Solution.
2021-12-16 3:05 AM
Hello @Entony and welcome to the Community :)
What Cubeprogrammer version are you used ? Please make sure to use the latest release.
Imen
2021-12-16 3:05 AM
Hello @Entony and welcome to the Community :)
What Cubeprogrammer version are you used ? Please make sure to use the latest release.
Imen
2021-12-16 10:39 PM
We had an old version, v2.8.0. Now we have a new version v2.9.0 and it works fine!
Thanks for the warning and I'm sorry, that should have occurred to me.;)