2024-03-17 5:15 AM
When I try to program my Blue Pill over UART in the Stm32CubeProgrammer it give me this Error message:
13:11:23 : Serial Port ttyUSB0 is successfully opened.
13:11:23 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1,0, flow-control = off
13:11:23 : Activating device: OK
13:11:23 : Board : --
13:11:23 : Chip ID: 0x410
13:11:23 : BootLoader protocol version: 3.0
13:11:23 : UPLOADING OPTION BYTES DATA ...
13:11:23 : Bank : 0x00
13:11:23 : Address : 0x1ffff800
13:11:23 : Size : 16 Bytes
13:11:23 : UPLOADING ...
13:11:23 : Size : 1024 Bytes
13:11:23 : Address : 0x8000000
13:11:23 : Read progress:
13:11:23 : Data read successfully
13:11:23 : Time elapsed during the read operation is: 00:00:00.106
13:11:54 : Memory Programming ...
13:11:54 : Opening and parsing file: blinky-test-f1-1.5.hex
13:11:54 : File : blinky-test-f1-1.5.hex
13:11:54 : Size : 12,47 KB
13:11:54 : Address : 0x08000000
13:11:54 : Erasing memory corresponding to segment 0:
13:11:54 : Erasing internal memory sectors [0 7]
13:11:54 : Erasing memory corresponding to segment 1:
13:11:54 : Erasing internal memory sectors [8 12]
13:11:54 : Download in Progress:
13:11:55 : File download complete
13:11:55 : Time elapsed during download operation: 00:00:01.549
13:11:55 : Verifying ...
13:11:55 : Read progress:
13:11:57 : Download verified successfully
13:11:57 : RUNNING Program ...
13:11:57 : Address: : 0x08000000
13:11:57 : Start operation achieved successfully
13:11:57 : Error: GETID command not acknowledged!
13:11:57 : Reemission of GetID command
13:11:57 : Error: GETID command not acknowledged!
13:11:57 : Reemission of GetID command
13:11:58 : Timeout error occured while waiting for acknowledgement.
13:11:58 : Error: GETID command not acknowledged!
13:11:59 : Timeout error occured while waiting for acknowledgement.
13:11:59 : Error: GETID command not acknowledged!
13:11:59 : Reemission of GetID command
13:12:00 : Timeout error occured while waiting for acknowledgement.
13:12:00 : Error: GETID command not acknowledged!
13:12:00 : Reemission of GetID command
13:12:01 : Timeout error occured while waiting for acknowledgement.
13:12:01 : Error: GETID command not acknowledged!
13:12:02 : Timeout error occured while waiting for acknowledgement.
13:12:02 : Error: GETID command not acknowledged!
13:12:02 : Reemission of GetID command
13:12:03 : Timeout error occured while waiting for acknowledgement.
13:12:03 : Error: GETID command not acknowledged!
13:12:03 : Reemission of GetID command
13:12:04 : Timeout error occured while waiting for acknowledgement.
13:12:04 : Error: GETID command not acknowledged!
13:12:05 : Warning: Connection to device 0x410 is lost
13:12:05 : Disconnected from device.
How do I fix this?
Solved! Go to Solution.
2024-03-21 4:10 AM
I made my own Blink program in the Arduino IDE:
// the setup function runs once when you press reset or power the board
void setup() {
// initialize digital pin LED_BUILTIN as an output.
pinMode(PC13, OUTPUT);
}
// the loop function runs over and over again forever
void loop() {
digitalWrite(PC13, HIGH); // turn the LED on (HIGH is the voltage level)
delay(1000); // wait for a second
digitalWrite(PC13, LOW); // turn the LED off by making the voltage LOW
delay(1000); // wait for a second
}
And that one worked, PC13 was blinking.
I uploaded it using Arduino IDE.
I also tried exporting the binary from Arduino IDE and Uploading using Stm32Cube Programmer, that also worked.
2024-03-17 6:45 AM
There is nothing to be fixed - the operation is correct.
2024-03-17 6:47 AM
You can try stm32flash.
2024-03-17 7:02 AM
When i try stm32flash i get this error:
stm32flash 0.7
http://stm32flash.sourceforge.net/
Using Parser : Intel HEX
Location : 0x8000000
Size : 12904
Error probing interface "serial_posix"
Cannot handle device "/dev/ttyUSB"
Failed to open port: /dev/ttyUSB
2024-03-17 7:34 AM
When your program is running, the UART connection isn't active. You need to boot up into the bootloader again to access the chip.
UART is not a viable debugging strategy. Get a nucleo or other board that uses an SWD connection.
2024-03-17 10:37 AM
You need a PC-Serial adapter to connect between the PC and the serial lines of the bootloader. You need to provide the devicename of the adapter.
2024-03-18 8:38 AM
I am using a UART to Usb Adapter.
2024-03-18 8:43 AM
How do I boot up into the bootloader to access the chip?
My Project requires a Blue Pill.
The Blue Pill also has SWD Pins, but I don't have an ST-Link.
2024-03-18 8:46 AM
The STM32 Cube Programmer also says that UART is Connected when I click the Connect button.
2024-03-18 8:56 AM - edited 2024-03-18 9:05 AM
@super_EEG wrote:I don't have an ST-Link.
Then you really should get one!
They really are invaluable in the ease of programming and debug access that they give you !
Don't tie your own hands behind your back - get an ST-Link* (or a Nucleo board).
@super_EEG wrote:My Project requires a Blue Pill.
Why?
It's just a board with a chip on it; it doesn't give you anything special or magic that a Nucleo or Discovery board wouldn't have, but the Nucleo does give you very significant advantages:
* Other debug probes are available.