2022-11-21 2:02 AM
Hi,
I am using STM32L071 micro controller for my product. We planned to flash the code using USART communication. The USART1 from MCU is connected to embedded system ( Nvidia Xavier NX ) using USB to UART converter. Then the MCU is put into boot mode by setting BOOT0 pin HIGH.
I confirmed that the MCU entered bootloader mode by connecting ST-Link V2 with the MCU and ensured that the PC pointed to the bootloader address(0X1FF00B38) of the STM32L071 series as shown in the image belowAfter entering system memory mode, if I try to flash the code through UART using STflash tool from Source Forge , I was not able to flash the code. Error shown by the program: Timed out.
Can someone please guide me what I am missing here?
Solved! Go to Solution.
2022-12-20 6:24 AM
Make sure to use a USB to Serial using CMOS levels, not RS232
Use a common ground
Ensure no other devices are signalling the STM32 immediately after reset.
The connection is one-shot, if it fails reset and try again.
2022-11-21 6:44 AM
First check if you can flash over STMCubeproggrammer using UART
2022-11-25 1:27 AM
Yes, I tried to flash using STMCubeprogrammer and that too failed with error.
2022-11-28 7:04 AM
Hello @Manoj_Guha_49,
Could you see if you encounter the same issue using STM32CubeProgrammer v2.12.0? You can download the latest release under this link.
If the same issue is encountered, could you share the verbose 3 log file from STM32CubeProgrammer? You can change the verbosity level using this radio button.
Thanks,
Aziz
2022-12-20 6:18 AM
Hi @Aziz BRIGUI ,
Please find the attached image when trying to flash thought UART mode with Verbosity level set to 3. I had verified that the PC is at 0x1FF00510 ( System memory ) when trying this method. I have also tried with different baud rates and parity set to "even", after that also I am getting the same error. Any help for this is very much appreciated. Thanks
2022-12-20 6:24 AM
Make sure to use a USB to Serial using CMOS levels, not RS232
Use a common ground
Ensure no other devices are signalling the STM32 immediately after reset.
The connection is one-shot, if it fails reset and try again.
2022-12-20 7:14 AM
Are you sure you connect to pins desired
and parity from your screenshot is none . Setup all ok and it work.
2023-01-22 8:31 PM
@Community member Thank you very much for the help. After ensuring the following aspects programming using UART was successful:
BTW I am using RS422 for programming and not TTL and it is working fine. We can close this issue.