2022-08-01 2:49 AM
I can control the card with stm32 CubeProgrammer when I reset mode "hardware reset". But when I use cubeIDE, I can't assign the program, it can't see the target, what could be the reason? Can I only use it in Hex mode?
Solved! Go to Solution.
2022-08-01 5:22 AM
Looks to be working
The "Programming" / "Downloading" is the second icon down on the left edge
Then you can specify your .HEX .ELF or .BIN file and program / verify from there.
Perhaps review a manual, videos or tutorials
2022-08-01 2:51 AM
with stm32 cubeprogrammer
2022-08-01 5:22 AM
Looks to be working
The "Programming" / "Downloading" is the second icon down on the left edge
Then you can specify your .HEX .ELF or .BIN file and program / verify from there.
Perhaps review a manual, videos or tutorials
2022-08-30 7:02 AM
Hello @buccno
Did the proposed solution came to help?
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.