2018-07-16 7:12 AM
Hello,
for the H743, the Stm32CubeProgrammer lists Option-Bytes->User Configuration->IWDG1 as 'Unchecked: Controlled by software' and 'Checked: Controlled by Hardware'. However the meaning is inverted! With IWDG1 unchecked, I can see a Reset every 500 ms even for an empty device.
The unexpected resets costed me hours!
Please correct a.s.a.p.
#stm32cubeprogrammer2018-08-08 7:03 AM
Bumping to remove from the home page (No Answer Posts)
2018-08-08 8:51 AM
An answer or some kind of confirmation is still welcome!
2018-08-08 9:43 AM
Sorry about that, smarter software would not clutter up my feed with posts I've already read/visited. The mute option seems to have no impact.
@ST Community
2018-08-16 1:25 AM
Hello,
Description of IWDG will be fixed and released in v1.1.1.
With Regards,
Imen