2022-09-29 12:57 AM
Dear all
If we clear the IWDG option (enable watchdog by hardware at bootup), we cannot undo this.
In that case we have to use the old STM32 ST-LINK Utility tool.
STM32CubeProgrammer version: v2.11.0
µC: STM32G474RBT3
The problem seems to be PC dependent!
Thanks in advance,
Franz
2022-09-29 06:30 AM
Hi @FWege.1 ,
I'm not able to reproduce the issue, can you please tell me more about your PC configuration where this issue occurs?
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer-2.11.0-RC4\bin>STM32_Programmer_CLI.exe -c port=SWD -ob IWDG_SW=1
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0-RC4
-------------------------------------------------------------------
ST-LINK SN : 001900303137510839383538
ST-LINK FW : V3J9M3
Board : STM32G474E-EVAL
Voltage : 3.28V
SWD freq : 24000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x469
Revision ID : Rev B
Device name : STM32G47x/G48x
Flash size : 512 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 20 Bytes
██████████████████████████████████████████████████ 100%
Bank : 0x01
Address : 0x40022044
Size : 16 Bytes
██████████████████████████████████████████████████ 100%
Bank : 0x02
Address : 0x40022070
Size : 8 Bytes
██████████████████████████████████████████████████ 100%
OPTION BYTE PROGRAMMING VERIFICATION:
Option Bytes successfully programmed
Time elapsed during option Bytes configuration: 00:00:01.173
Houda
2022-09-29 04:20 PM
Connect mode: Under Reset
Reset mode : Hardware reset
2022-10-04 12:16 AM
Hello together
First thanks for your answers.
The problem occurs sporadically - mostly on the Windows 7 systems.
Betriebssystemname Microsoft Windows 7 Professional
Version 6.1.7601 Service Pack 1 Build 7601
Systemtyp x64-basierter PC
Maybe it has something to do with the watchdog – I’m not sure. How is the watchdog handled during programming/flashing?
The only difference in the logfiles is following line – which occurs on my windows 10 system, if everything works as expected
16:27:13:483 : WriteOB function terminated with connection error due to OB_Launch
Thanks Piranha – but unfortunately that doesn't help