cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer gives me an error

PNenn.1
Associate

I'm trying to program STM32L031 microcontroller using STLINK but STM32CubeProgrammer gives me the following error:

Error: No STM32 target found!

These are the conditions:

1) The hardware is correctly connected because the STM32CubeIde emulates correctly the target

2) I have updated the STLINK firmware to the last firmware release

3) I have tested the programmer on another computer and I get the same error

4) I already tested to power cycle several times the target and the emulator but nothing changes

Can someone help me?

Thanks in advance

Paolo

1 REPLY 1

Hi @PNenn.1​ 

Please try with the last STM32CubeProgrammer then tell me if it solve the issue.

Best regards,

Nesrine