cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer cannot connect to MCU using j-link

UniverGao
Associate

Version: v2.16.0

I`ve downloaded and installed the latest application and was told that the CubeProgrammer could support J-Link now.

the GUI shows that JLink device can be selected:

UniverGao_0-1715412382353.png

 

I clicked the connect bottom, the chip select window of JLink was popped out:

UniverGao_1-1715412644768.png

UniverGao_2-1715412669475.png

after correct chip was selected, the error window showed below:

UniverGao_3-1715412735928.png

the error logs like this:

 

 

 

  15:30:23 : UR connection mode is defined with the HWrst reset mode
  15:30:23 : 20730746
  15:30:23 : Error: J-Link - Connection to target failed
  15:30:23 : Error: J-Link - Reading CPUID failed
  15:30:23 : Voltage     : 3.30V
  15:31:20 : Error: Database cannot be found. DatabasePath = D:\ProgramFiles\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/../Data_Base/STM32_Prog_DB_0xFFF.xml
  15:31:20 : Error: flash loader cannot be loaded. FlashLoaderPath = D:\ProgramFiles\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0xFFF.stldr
  15:31:20 : Error: Database cannot be found. DatabasePath = D:\ProgramFiles\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/../Data_Base/STM32_Prog_DB_0xFFF.xml

 

 

 

 I wander if the app support jlink probe, if not, why I can select it?

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief II

I just tried on my Laptop here, no problem :

AScha3_0-1715417232756.png

AScha3_1-1715417283031.png

Its on Win 10 pro, 22H2 .

ed 

Just i remember : my J-link refused to connect to new H7 series, needs some update to connect to this.

So try connect with an "old" cpu, like the F103 i tested here, to check: problem with J-link version or other.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

13 REPLIES 13
AScha.3
Chief II

I just tried on my Laptop here, no problem :

AScha3_0-1715417232756.png

AScha3_1-1715417283031.png

Its on Win 10 pro, 22H2 .

ed 

Just i remember : my J-link refused to connect to new H7 series, needs some update to connect to this.

So try connect with an "old" cpu, like the F103 i tested here, to check: problem with J-link version or other.

If you feel a post has answered your question, please click "Accept as Solution".
Andrew Neil
Evangelist III

So can the J-Link connect using Segger's utilities?

 

Meganita
Associate II

Hello,

 

I'm having the same problem:

13:24:21 : STM32CubeProgrammer API v2.16.0 | Windows-64Bits
13:26:41 : UR connection mode is defined with the HWrst reset mode
13:26:41 : 52006738
13:26:41 : Error: J-Link - Connection to target failed
13:26:41 : Error: Unable to get Access port number
13:26:41 : Voltage : 3.30V
13:27:04 : Error: Database cannot be found. DatabasePath = C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/../Data_Base/STM32_Prog_DB_0xFFF.xml
13:27:04 : Error: flash loader cannot be loaded. FlashLoaderPath = C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0xFFF.stldr
13:27:04 : Error: Database cannot be found. DatabasePath = C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/../Data_Base/STM32_Prog_DB_0xFFF.xml

 

I found out that the correct database for the STM32 that I'm using (STM32L052K8) should be 0x417, not 0xFFF. Why does it want to choose 0xFFF?

 

You'll find the configuration I use below:

Meganita_0-1715686849910.png

 


@Meganita wrote:

I'm having the same problem:


So again the same question: 

Can the J-Link connect using Segger's utilities?

If not, Segger have some help on 'Cannot connect to Target' problems:

https://wiki.segger.com/J-Link_cannot_connect_to_the_CPU

 

See also this ST knowledgebase article on the subject:

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693

 

As you can see below, the connection between the PC and the J-Link is ok, but not the connection to the target. 

SEGGER J-Link Commander V7.96e (Compiled Apr 17 2024 16:26:32)
DLL version V7.96e, compiled Apr 17 2024 16:25:43

Connecting to J-Link via USB...O.K.
Firmware: J-Link V12 compiled Apr 15 2024 17:37:25
Hardware version: V12.00
J-Link uptime (since boot): 0d 00h 00m 03s
S/N: 52006738
License(s): GDB
USB speed mode: High speed (480 MBit/s)
VTref=3.300V (fixed)


Type "connect" to establish a target connection, '?' for help
J-Link>connect
Please specify device / core. <Default>: STM32L052K8 (ALLOW OPT. BYTES)
Type '?' for selection dialog
Device>
Please specify target interface:
  J) JTAG (Default)
  S) SWD
  T) cJTAG
TIF>S
Specify target interface speed [kHz]. <Default>: 4000 kHz
Speed>
Device "STM32L052K8 (ALLOW OPT. BYTES)" selected.


Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -> SWD switching sequence.
Error: Failed to initialized DAP.
Can not attach to CPU. Trying connect under reset.
SWD selected. Executing JTAG -> SWD switching sequence.
Error: Failed to initialized DAP.
Connecting to CPU via connect under reset failed.
InitTarget() end - Took 308ms
Connect failed. Resetting via Reset pin and trying again.
InitTarget() start
SWD selected. Executing JTAG -> SWD switching sequence.
Error: Failed to initialized DAP.
Can not attach to CPU. Trying connect under reset.
SWD selected. Executing JTAG -> SWD switching sequence.
Error: Failed to initialized DAP.
Connecting to CPU via connect under reset failed.
InitTarget() end - Took 308ms
Error occurred: Could not connect to the target device.
For troubleshooting steps visit: https://wiki.segger.com/J-Link_Troubleshooting
J-Link>

I suppose that "DAP" is "Database Path". 

As per the first link you provided, I have checked VTREF. It is 3.3 V.

I have also reduced the speed down to 100 kHz, but I still have the same error.

As per the second link you provided, SWDIO and SWCLK are "used by the debug".


@Meganita wrote:

I suppose that "DAP" is "Database Path". 


No.

The DAP is the Debug Access Port - the part of the CPU which actually connects to the debug probe:

https://developer.arm.com/documentation/102585/0100/What-is-a-Debug-Access-Port-

https://wiki.segger.com/DAP 

So your J-Link is fundamentally failing to connect to the target - it's not related to the CubeProgrammer.

Does your code disable or repurpose the debug lines (SWDIO, SWCLK), and/or put the CPU to sleep?

 

EDIT:

Example showing the Debug Access Point (Debug AP) - DAP:

AndrewNeil_0-1715699714928.png

 

EDIT 2:

Did you note @AScha.3 comment at the end of this post:

https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-cannot-connect-to-mcu-using-j-link/m-p/672940/highlight/true#M6415

Does your J-Link connect to any other STM32 targets?

Also, do you have an ST-Link to try? Or a different J-Link?

Andrew Neil
Evangelist III

@UniverGao - did you resolve your issue?

What chip specifically are you using?

Show wiring for complete debug harness.

What model of Segger J-Link?

USB 2.0 high speed rated cable? Direct connection, not via hub or docking station?

Is this demonstrably working on a known working board / debug harness?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

No, SWDIO and SWCLK aren't repurposed or disabled. The CPU is not put to sleep.

We don't have any other product with an STM32, so I cannot try to connect to another STM32. 

And I don't have an ST-Link nor another J-Link...

 

@Tesla DeLorean 

I'm using STM32L052K8, with J-Link Base. USB 2.0 through direct connection (no hub, no docking station). 

I have VTREF connected on pin 1, VSS connected on pin 4, SWDIO on pin 7, SWCLK on pin 9 and RESET on pin 15.

I don't have another board to try it on.