2020-05-31 06:06 PM
[ The text uses a translation tool. ]
Flash size is the default and no more programs can be loaded.
environment
Windows10 + STM32CubeMX + ST-Link2
************** Console log
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 53FF6D064882505226101587
ST-LINK FW : V2J36S7
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x436
Device name : STM32L15xxD/STM32L162xD
Flash size : 128 KBytes (default)
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a20796.srec
File : ST-LINK_GDB_server_a20796.srec
Size : 137888 Bytes
Address : 0x08010000
Erasing memory corresponding to segment 0:
Error: Operation exceeds memory limits
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
*************
I'm using an STM2L151DTx, so there's plenty of flush
Why is it [Flash size: 128 KBytes (default)]?
The STM32 ST-LINK Utility can be recognized and written normally.
Am I doing something wrong?
2021-06-03 02:23 AM
Hello @FARSL.1 ,
First of all Welcome to ST Community!
In order to ensure a follow-up of your request, could you please submit it in a new thread?
You can provide link to current question if you think that both cases are similar.
Thanks for your understanding!
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-06-04 03:43 AM
Thanks for your answer @Amel NASRI .
I did not want to open another thread. Because I get same problem with @高橋 �?�一 . This problem still going on. I could not find any solutions about wrong flash size detect.
2021-06-05 03:01 AM
The same tool, the same MCU and the same bug - incorrect flash size. It does not need a new thread, because at least from a user's perspective it is exactly the same issue, which is still not fixed or has been broken again.
2021-06-09 09:53 AM
OK then let us keep it here 🙂 and ping our STM32CubeProgrammer Expert (@Houda GHABRI ) in order to provide a status for this issue.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-06-10 01:05 AM
Hi @FARSL.1 ,
I confirm for STM32L151RD (Device ID 0x436 ) there is an issue of Flash size :128KB displayed in STM32CubePRogrammer instead of 384KB.
This issue is already under debugging by CubePRogrammer development team and will be fixed soon.
I will come back with the latest updates.
Hope this helps you.
Houda
2021-06-24 08:31 AM
Hello I have the same problem.
I contacted you about this maybe 6-7 months ago. Can you even imagine all the trouble i had to deal with? I couldnt debug my software fully. I had to comment out some parts in order to use debugger with STM32 cubeMX ide.
Check out my post
How can you be so neglecting I jsut dont get it.
Please find a solution to this issue. When will you do this?
Thanks
2021-06-24 08:55 AM
Workaround: use ST-LINK_CLI.exe or the gdb debugger built into the IDE rather than STM32CubeProgrammer.
2021-08-17 02:26 AM
Hello ST Team,
Any fixes on this issue?
Thank you.
2021-08-17 02:42 AM
Hi @herca.1 ,
Did you try with the last CubeProgrammer version 2.8.0 ?
Issue should be fixed in this release.
Houda
2021-08-17 04:43 AM
Hello,
Using 2.8.0 and using STM32L15xx microcontroller
This is the output of Cube Programmer. Verbosity level 3. Is this also fixed for CubeMX IDE, I want to be able to debug my software.
14:40:51:303 : Size : 263956 Bytes
14:40:51:303 : Address : 0x08000000
14:40:51:303 : Erasing Segment <0> Address <0x08000000> Size <263956>Bytes
14:40:51:303 : Erasing memory corresponding to segment 0:
14:40:51:303 : Memory erase...
14:40:51:322 : halt ap 0
14:40:51:322 : w ap 0 reg 15 PC (0x20000000)
14:40:51:331 : w ap 0 reg 17 MSP (0x20000500)
14:40:51:331 : w ap 0 reg 16 xPSR (0x01000000)
14:40:51:336 : w ap 0 @0x20000E20 0x00000200 bytes Data 0x00000000
14:40:51:336 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
14:40:51:362 : w ap 0 @0x20000004 0x000009EC bytes Data 0xF8DFB580
14:40:51:363 : Error: Operation exceeds memory limits
14:40:51:381 : Error: failed to erase memory