2022-07-26 12:08 AM
Trying the program STM32H750B-DK discovery board using STM32CubeProgrammer, but it fails. Here is the log:
08:47:43 : STM32CubeProgrammer API v2.11.0 | Linux-64Bits
08:47:45 : ST-LINK SN : 0036004A3137511133333639
08:47:45 : ST-LINK FW : V3J10M3
08:47:45 : Board : STM32H750B-DK
08:47:45 : Voltage : 3,28V
08:47:45 : SWD freq : 24000 KHz
08:47:45 : Connect mode: Normal
08:47:45 : Reset mode : Software reset
08:47:45 : Device ID : 0x450
08:47:45 : Revision ID : Rev V
08:47:45 : Debug in Low Power mode is not supported for this device.
08:47:46 : UPLOADING OPTION BYTES DATA ...
08:47:46 : Bank : 0x00
08:47:46 : Address : 0x5200201c
08:47:46 : Size : 308 Bytes
08:47:46 : UPLOADING ...
08:47:46 : Size : 1024 Bytes
08:47:46 : Address : 0x8000000
08:47:46 : Read progress:
08:47:46 : Data read successfully
08:47:46 : Time elapsed during the read operation is: 00:00:00.002
08:47:53 : Memory Programming ...
08:47:53 : Opening and parsing file: GPIO_IOToggle.hex
08:47:53 : File : GPIO_IOToggle.hex
08:47:53 : Size : 4,56 KB
08:47:53 : Address : 0x90000000
08:47:53 : Erasing memory corresponding to segment 0:
08:47:53 : Download in Progress:
08:47:53 : Error: failed to download Segment[0]
08:47:53 : Error: failed to download the File
08:53:41 : Disconnected from device.
Solved! Go to Solution.
2022-07-27 1:25 AM
Hi,
For a reason I ignore I cannot answer on the other thread so let me answer you here:
As mentioned in the other thread, the workaround mentioned by @Community member is only relevant for custom external loaders. When using an ST development kit such as the STM32H750B-DK you just need to select the proper external loader in the "EL" tab of the CubeProgrammer :
STM32CubeIDE include its own version of CubeProgrammer so the same applies, open the Debug Configuration, go the the "Debugger" tab, then :
See details in section 3.4.1 (Revision 6) of the STM32CubeIDE user manual
Best regards,
Nicolas
2022-07-26 5:37 AM
This was a similar thread
https://community.st.com/s/question/0D53W00001cIHMQSA4/external-loader-fails-to-download
@N. SANTINI
2022-07-27 1:25 AM
Hi,
For a reason I ignore I cannot answer on the other thread so let me answer you here:
As mentioned in the other thread, the workaround mentioned by @Community member is only relevant for custom external loaders. When using an ST development kit such as the STM32H750B-DK you just need to select the proper external loader in the "EL" tab of the CubeProgrammer :
STM32CubeIDE include its own version of CubeProgrammer so the same applies, open the Debug Configuration, go the the "Debugger" tab, then :
See details in section 3.4.1 (Revision 6) of the STM32CubeIDE user manual
Best regards,
Nicolas
2022-07-27 1:33 AM
Thanks, it helped!
2022-07-27 3:12 AM
I'm not sure why the programming gets this deep into the process without flagging it doesn't have a loader covering the address space in question.
It's a bit like reading 64MB of data before reporting a failure in the first block.
These are things surely that could be caught earlier, and with clear and specific error messages?
2022-07-27 4:28 AM
I agree, this has already been reported internally.
Best regards,
Nicolas
2022-12-12 4:26 AM
Internal ticket number: 132409 (This is an internal tracking number and is not accessible or usable by customers).
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.