2023-12-28 8:01 AM - edited 2023-12-28 8:06 AM
I've got a brand new VM running Windows 11 pretty much off the shelf. I can install and run Cube IDE but when I try to install the STM32CubeProgrammer (64 bit version) I get into an infinite loop where the following happens:
- It opens the Install Wizard which then closes
- It opens the blue "STM32 Cube Programmer" window, which then closes
- It opens the Install Wizard which then closes
Here is a video of the behavior: https://www.loom.com/share/b3ce5e7a79ad425d840296845fd0c1ed
The only way I can exit this loop is to reset the whole machine. It's not installed, so I can't uninstall it. I tried removing everything, upgrading java, and still the same problem. Any suggestions would be appreciated. Thank you!
2024-02-01 2:37 AM
Hello @thayden,
Sorry for the late reply.
I have tested the installation of STM32CubeProg 2.15.0 on Windows 11 and did not encounter the issue described. I even tried with a freshly installed VM, and everything seems to be working fine. Did the same behavior occur with older versions ?
Maryem.
2024-03-19 6:51 PM
Just an update:
Problem is still there using new version STM32CubeProgrammer v2.16.0. After installing, the program is not responding after I click OK button. See attached pic.
I need to force close from task manager. The next time I run the CubeProgrammer, it auto-closed by itself after showing the blue welcome screen for about 2 seconds.
At least the workaround method is still working:
jre\bin\java.exe -Djna.nosys=true -jar STM32CubeProgrammer.exe
2024-09-09 10:14 AM
I encountered the same issue on a freshly setup Windows 11 VM.
I was finally able to get the installation to go through by somewhat dumb luck. I'm not sure if it's reproducible because the process was too annoying to bear repeating. I got it to interrupt the loop by ctrl-alt-del in host followed by vm.
I tried most combinations of the following versions of installer/jre in 32 and 64 bit: **
installers:
en.stm32cubeprog_v2-5-0 *** |
en.stm32cubeprg-win64_v2-7-0 |
en.stm32cubeprg-win64-v2-17-0 |
en.stm32cubeprg-win32_v2-7-0 |
en.stm32cubeprg-win32-v2-17-0 |
system java installed ****
none (both before installing any version of java and after removing JAVA_HOME and all java/bin from PATH) |
openjdk 1.8.0_265 (extracted from bundled cubeprg-win64_v2-7-0 installer) |
amazon-corretto-8.422.05.1-windows-x86-jre |
amazon-corretto-8.422.05.1-windows-x86-jdk |
amazon-corretto-8.422.05.1-windows-x64-jre |
amazon-corretto-8.422.05.1-windows-x64-jdk |
openjdk-11.0.2_windows-x64_bin |
openjdk-17.0.2_windows-x64_bin |
amazon-corretto-21.0.4.7.1-windows-x64-jdk |
openjdk-22.0.2_windows-x64_bin |
* note: The installer should not require any jre/jdk, but I experimented with many different versions because it seemed like javaw was crashing while starting the installer.
** in addition to underlying system java, I experimented with extracting the original stm32cubeprogrammer installer .exes and replacing the contained jre with various versions from above before running the extracted .exe
*** note: does not come bundled with jre. fails to start, citing requiring JRE 1.8.0_66-10.99.99. Attempted with jre/jdk 1.8.0_422, and jre 11, 17, 21, 22
**** note: java installed by unzipping to a specified folder and updating PATH and JAVA_HOME sys/environment variables