2020-02-20 3:15 AM
I have installed the latest (en.stm32cubeprog_v2-3-0) version in Windows 10 64 bit PC.
After installation, the first startup icon with spinner only comes up , closes and does not run.
As far as googled and found online, it is java versioning issue. This is not new. Last version also, I had to manually kill the Java process from Task Manager, and then re-opening used to run.
Now, I don't see a Java process itself.
Given there are variety of Java versions, environments, when will you fix your CubeProgrammer dependency path settings, so that it looks at correct place !?
Java versions in my PC are:
C:\Program Files\Java>dir
Directory of C:\Program Files\Java
27/01/2020 10:29 <DIR> .
27/01/2020 10:29 <DIR> ..
05/07/2018 14:17 <DIR> jdk-10.0.1
22/10/2018 08:19 <DIR> jdk-11.0.1
27/08/2019 09:02 <DIR> jdk-11.0.4
27/08/2019 08:59 <DIR> jdk-12.0.2
14/11/2018 09:43 <DIR> jdk1.8.0_192
27/08/2019 09:00 <DIR> jdk1.8.0_221
27/01/2020 10:29 <DIR> jre1.8.0_231
27/01/2020 10:29 <DIR> jre1.8.0_241
C:\Program Files (x86)\Java>dir
Directory of C:\Program Files (x86)\Java
27/01/2020 10:29 <DIR> .
27/01/2020 10:29 <DIR> ..
27/08/2019 09:01 <DIR> jdk1.8.0_221
27/01/2020 10:29 <DIR> jre1.8.0_241
And then environment
C:\Program Files\Java>set
...
JAVA_HOME=C:\Progra~1\Java\jdk1.8.0_221
...
....
Path=C:\Program Files (x86)\Common Files\Oracle\Java\javapath; ....
I understand STM32CubeProgrammer release note (RN0109) and UM2237 User manual for STM32CubeProgrammer en.DM00403500.pdf both mentions of Host PC System requirements for Java.
Would you please fix this "basic" issue ??
2020-10-30 5:24 AM
Hello @PPK
Thanks for the feedback,
For STM32CubeProgrammer tool, STMicroelectronics recommend to use the Zulu 8 JRE .
Development team is working on bundling the JRE with STM32CubeProgrammer 2.6.0 installer", there will be no more need to install a JRE to use STM32CubeProgrammer.
Best regards,
Nesrine