2020-11-19 05:00 PM
Is it possible to write data by using CubeProgrammer or ST-LINK utility?
I am thinking if software created in other project can be written or marged by using any application or not.
Solved! Go to Solution.
2020-11-19 05:44 PM
Those programs both read/write firmware to/from the chip. They're not designed to communicate with a program already running on the chip, if that's what you're asking.
2020-11-19 05:44 PM
Those programs both read/write firmware to/from the chip. They're not designed to communicate with a program already running on the chip, if that's what you're asking.
2020-11-19 09:02 PM
To TDK
Thank you for your comment.
I will be explaining what I am trying below.
Here is a problem.
I created boot program and main program. They are created separately and after tried to merge them.
However, I got mistake. Before boot program became perfect, I merged it with main program and then I cannot update software from SD card anymore.
The only way that I can update is to update onboard.
That is why I would like to prevent it from mistake and I am looking for the preventive measure.
2020-11-25 06:23 PM
I might be able to figure this out by using CLI on CubeProgrammer or ST-LINK utility.
Thank you for your support.