2021-12-07 6:20 AM
Hi
The command to download our firmware is as follow (with the option bytes display to show that protection is disabled):
STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -ob displ -e all -d C:\Temp\cu.hex -d C:\Temp\data.hex -v -rst
The result always gives an error for the flash mass-erase:
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0
-------------------------------------------------------------------
ST-LINK SN : 31FF6E064D4E353821590843
ST-LINK FW : V2J29S7
Board : --
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x418
Revision ID : Rev Z
Device name : STM32F105/F107 Connectivity Line
Flash size : 256 KBytes
Device type : MCU
Device CPU : Cortex-M3
BL Version : --
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x4002201c
Size : 8 Bytes
██████████████████████████████████████████████████ 100%
Bank : 0x01
Address : 0x1ffff800
Size : 16 Bytes
██████████████████████████████████████████████████ 100%
OPTION BYTES BANK: 0
Read Out Protection:
RDP : Disabled (Flash memory is not read-protected.)
User Configuration:
WDG_SW : 0x1 (Software watchdog)
nRST_STOP : 0x1 (No reset generated)
nRST_STDBY : 0x1 (No reset generated)
User Data:
Data0 : 0xFF (0xFF)
Data1 : 0xFF (0xFF)
Write Protection:
WRP0 : 0x1 (Write protection not active on this sector)
WRP1 : 0x1 (Write protection not active on this sector)
WRP2 : 0x1 (Write protection not active on this sector)
WRP3 : 0x1 (Write protection not active on this sector)
WRP4 : 0x1 (Write protection not active on this sector)
WRP5 : 0x1 (Write protection not active on this sector)
WRP6 : 0x1 (Write protection not active on this sector)
WRP7 : 0x1 (Write protection not active on this sector)
WRP8 : 0x1 (Write protection not active on this sector)
WRP9 : 0x1 (Write protection not active on this sector)
WRP10 : 0x1 (Write protection not active on this sector)
WRP11 : 0x1 (Write protection not active on this sector)
WRP12 : 0x1 (Write protection not active on this sector)
WRP13 : 0x1 (Write protection not active on this sector)
WRP14 : 0x1 (Write protection not active on this sector)
WRP15 : 0x1 (Write protection not active on this sector)
WRP16 : 0x1 (Write protection not active on this sector)
WRP17 : 0x1 (Write protection not active on this sector)
WRP18 : 0x1 (Write protection not active on this sector)
WRP19 : 0x1 (Write protection not active on this sector)
WRP20 : 0x1 (Write protection not active on this sector)
WRP21 : 0x1 (Write protection not active on this sector)
WRP22 : 0x1 (Write protection not active on this sector)
WRP23 : 0x1 (Write protection not active on this sector)
WRP24 : 0x1 (Write protection not active on this sector)
WRP25 : 0x1 (Write protection not active on this sector)
WRP26 : 0x1 (Write protection not active on this sector)
WRP27 : 0x1 (Write protection not active on this sector)
WRP28 : 0x1 (Write protection not active on this sector)
WRP29 : 0x1 (Write protection not active on this sector)
WRP30 : 0x1 (Write protection not active on this sector)
WRP31 : 0x1 (Write protection not active on this sector)
Erase sector(s) ...
Error: Mass erase operation failed.
Please verify flash protection
Memory Programming ...
Opening and parsing file: cu.hex
File : cu.hex
Size : 32 KBytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 15]
Download in Progress:
██████████████████████████████████████████████████ 100%
File download complete
Time elapsed during download operation: 00:00:01.725
Memory Programming ...
Opening and parsing file: data.hex
File : data.hex
Size : 8 Bytes
Address : 0x08007000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 14
Download in Progress:
██████████████████████████████████████████████████ 100%
File download complete
Time elapsed during download operation: 00:00:00.095
Verifying ...
Read progress:
██████████████████████████████████████████████████ 100%
Download verified successfully
MCU Reset
Software reset is performed
When I replace the mass-erase with the request to only erase the sectors of interest (-e [0 15], I got no error but also no guarantee of the operation done:
Existing specified sectors are erased successfully
Protected sectors are not erased
Additional info: if the erase step is not provided, the failure happens while attempting erasing sectors before the first download.
Why this error ?
Many thanks in advance.
Regards