cancel
Showing results for 
Search instead for 
Did you mean: 

Can't close app, if connection was failed.

PGorb.1
Associate

Hello, i found next problem. If open app, and try connect to board with unsuccessful result, than app can't be closed any method, other than via task manager. In other case, app close via stantard button. This bug not disapering, if, for example, first try was failed, but few try later was successful. OS Windows 10 x64 (with last update at time of writing this topic). Tested chips: STM32L053 (custom board), STM32F031(NUCLEO-F031K6) .

15 REPLIES 15

Hi @PGorb.1​ 

Please try with the last CubeProgrammer version (2.5.0) then tell me if it solve the issue.

Best regards,

Nesrine

Radosław
Senior II

Same problem also with 2.5.0. despribed earlier on this forum.

Hello @Rados?aw​ 

Tested the same scenario without getting issue. Please try to upgrade Firmware then tell me if the issue still exist.

0693W000005A9UKQA0.pngBest regards,

Nesrine

Radosław
Senior II

I use latest firmware.

I notice something else, config.properties file is empty

Could you please specify the board name.

PS. Tested on new computer with win 10 pro, also 2 colleagues have same effect.
Radosław
Senior II

Tested with STLINK V2-1 and V3. target must be unconnected

Radosław
Senior II

Next situation. Afted this blocked state, config.properties is empty, Next time with no stlink connected to PC i click connect, then config.properties include soome options. then ONLY ONES cube prog can be closed after failure conection to target.

Hi @Rados?aw​ 

Please check cables, a lot of people use ST-Link with success, so i think the problem is on your side.

0693W000005AHfLQAW.pngBest regards,

Nesrine