2023-04-13 1:44 AM
Hi,
On my Nucleo-F756ZG, when I generate code for USART3 that's by default connected to ST-LINK , Cube sets pins for morpho connector (PB10 PB11) instead of alternate function (PD8 PD9). I also use Nucleo-L476RG and for this board, Cube set alternate funtion pin for Usart2 default connected to ST-LINK.
2023-04-20 12:40 AM
@Ghofrane GSOURI ?
2023-04-27 2:45 AM
@Ghofrane GSOURI ? Could you answer?
2023-04-27 4:36 AM
@Sara BEN HADJ YAHYA
Not sure whom to flags this with.
Needs some Board Level Awareness related to suggested pin defaults for peripherals. Will lead to less mistakes, and more code working on first try.
2023-04-27 5:41 AM
Hello @Community member ,
@Ghofrane GSOURI will investigate this issue and provide an answer asap.
Sara.
2023-05-11 3:26 AM
what's up?
2023-05-11 6:40 AM
Hello @Kamil Duljas
Sorry for the late response.
Your suggestion is submitted to dev team .
Internal ticket number: 151857(This is an internal tracking number and is not accessible or usable by customers).
I will keep you posted with updates.
Thx
Ghofrane
2023-05-11 6:41 AM
Thanks :folded_hands: