Solved
writing to timer CR1 register before MX_TIM_Init() doesn't work
Hello!
Can anybody explain to me why the following code is not writing to the TIM2 and TIM3 CR1 register:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* timers will only generate an UI when the counter wraps around */
TIM2->CR1 |= TIM_CR1_URS;
TIM3->CR1 |= TIM_CR1_URS;
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_OPAMP1_Init();
MX_OPAMP2_Init();
MX_TIM2_Init();
MX_TIM15_Init();
MX_USB_DEVICE_Init();
MX_TIM3_Init();
/* USER CODE BEGIN 2 */but when I move the register writes after the peripheral initializations it works:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_OPAMP1_Init();
MX_OPAMP2_Init();
MX_TIM2_Init();
MX_TIM15_Init();
MX_USB_DEVICE_Init();
MX_TIM3_Init();
/* USER CODE BEGIN 2 */
/* timers will only generate an UI when the counter wraps around */
TIM2->CR1 |= TIM_CR1_URS;
TIM3->CR1 |= TIM_CR1_URS;I don't understand this.
best regards
Benjamin