Skip to main content
October 28, 2019
Question

Not running NAND FLASH with STM32H70VB

  • October 28, 2019
  • 1 reply
  • 587 views

Hi,

I have a Project which is about data transfering and storaging.

I use STM32H750VB micro processor, MT29F32G08CBADBWP-12IT:D Nand Flash and LAN8742A Ethernet Chip for my application.

I configure and run Ethernet, ADC, I/O, UART etc. functions with using CubeMX. However I had some problems on Nand Flash application while was trying tu run it.

I did run the Nand Flash application correct when I used STM32F407 Discovery MB997B development kit.

I couldn’t find yet any example about H743ZI development kit.

1-     Do you have any experience about programming Nand Flash application with using H743ZI development kit.

2-     Do you have any idea "MPU - Memory Protection Unit" inside micro processor.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
November 11, 2019

Think you're going to need to own the coding/porting of drivers for this. People generally have migrated to eMMC to solve a host of issues from EOL form factors, architecture/geometry issues, and wear levelling.

Yes, you probably want to use the MPU, don't want buffering or caching on NAND space. Review books or manuals on CM7 core, or CPU architecture/design, if unfamiliar with the topic area.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..