2019-07-26 6:14 PM
After Oracle announcement related to ‘End of Public Updates for Oracle JDK 8’, you can access OpenJDK 8 via https://adoptopenjdk.net/. But it will not
2020-01-30 3:09 AM
Same for me, I installed the OpenJDK 8 JRE. The output of `java -version` is the following:
C:\>java -version
openjdk version "1.8.0_242"
OpenJDK Runtime Environment (AdoptOpenJDK)(build 1.8.0_242-b08)
OpenJDK 64-Bit Server VM (AdoptOpenJDK)(build 25.242-b08, mixed mode)
The Installation program of STM32CubeMX-5.5.0 opens a window with the message "This application requires a Java Runtime Environment 1.8.0_45". The installation does not continue.
2020-01-31 7:07 AM
I had a similar problem, but STM32CubeMX was already installed in my machine. I couldn't use the software after I removed Oracle JRE in favor of OpenJDK. The message was the same as yours: "This application requires a Java Runtime Environment 1.8.0_45".
However, after a lot of searching, I saw someone running an executable directly with java (I don't recall whether it was the setup file or the actual software executable). So, I opened a cmd at my installation directory and executed:
java -jar STM32CubeMX.exe
And it worked. After that, I edited my shortcut in desktop to use `java -jar` as well.
I suggest you try the same with the setup file.
By the way, I'm using OpenJDK 13.0.1 and it seems to work fine.
2020-02-05 4:28 AM
Interesting, I tried to install CubeMX with an Oracle Java installation, after uninstalling this and installing the AdoptOpenJDK, I tried to run it from the command line, but it was not working. After installing CubeMX with
java -jar SetupSTM32CubeMX-5.5.0.exe
from an administrator command line, I can now start CubeMX from the start menu without even changing the shortcut.
Sadly this does not work for the STM32CubeProgrammer.
2020-05-14 2:43 AM
To easily fix this, install AdoptOpenJDK with the following settings:
2020-08-26 8:05 AM
thanks @Community member lastly it work after installation of adoptOpenJDK.Thanks Alot