cancel
Showing results for 
Search instead for 
Did you mean: 

The bug in the "Commercial Part Number" field of stm32cubeMX.

Tuzki
Associate

Hi。

A simple yet glaring bug that persists: when you open stm32cubeMX and enter information in the 'Commercial Part Number' field, you'll notice that the letters you type appear twice. For example, if you type 's', the input box shows 'ss'; if you type 't', the input box shows two 't's.

 

Tuzki_0-1741412429811.png

-----warmest greetings

1 REPLY 1
Tuzki
Associate

This issue might not be easily discovered by others. I found that this bug only occurs when the input method is set to Chinese on a Windows system. For example, if my input method is currently set to Chinese and I type an 's' in the input box, the input box immediately makes the input method candidate selection bar disappear and then shows two 's's.