2019-06-11 8:31 AM
Hello,
I am attempting to use all 4 sai ports as one large synchronous audio device.
The I want SAI1A to be the master, and SAI1B, SAI2A, SAI2B, SAI3A, SAI3B, SAI4A, SAI4B to all be synchronous slaves to the SAI1A.
I am able to configure them all, except for SAI4B, which says it's in conflict with SAI1B synchronous slave. I'm using the internal synchronous signals, all synchronous slaves are marked as, "Synchronous with other SAI, SAI1". But just 4B says it's in conflict.
I assume if I configure it manually, it'll probably work fine...
Thanks
-Caleb
2019-06-28 2:54 AM
Hi @caleb ,
This issue seems to be similar to the one reported in this question.
I add @Khouloud ZEMMELI to let us know if there is any update on this regard.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-07-01 12:18 AM
Hello , For : this question : According to our development team, the product supports only 6 microphones.
Request invalid.
Regards,
Khouloud.
2019-07-01 1:53 AM
@caleb , could you please share more info about your request? which version of CubeMX?
Regards,
Khouloud.
2019-07-03 1:12 AM
hi @caleb , Tested with H743IIKx and it works fine , for H750 it will be fixed .
Best Regards,
Khouloud.