Question
When selecting CMSIS Core and DSP in CubeMX, via Software Packs, then click ok, save and generate code, nothing is added to project
I'm creating a STM32Cube project, for the STM32H7B3I-DK. When selecting CMSIS Core and DSP in CubeMX, via Software Packs, then click ok, save, generate code, nothing happens. CMSIS or DSP lib aren't added. No module appears in the Software Package section of the .ioc editor.
If I close eclipse and open it again, the selected package sections are gone, not saved with the project.
STM32CubeIDE Version: 1.4.2
STM32CubeH7 Firmware Package V1.8.0 / 29-May-2020
CMSIS Release version : 5.7.0 Release date : 2020-04-09