cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-C071RB - IAR "Non-recognized options in project file" during debugging

curiocity
Associate III

Hi,

Can you please help me for below  

I am using NUCLEO-C071RB development board ,I am generating the code using CUBE MX software(V6.14.1) following steps I have followed 

Step 1:Selected the board as NUCLEO-C071RB

Step 2:From project manager I have selected the Toolchain/IDE as EWARM and other configuration as below 

curiocity_1-1748855996589.png

Step 3:Clicked on generate code 

Step 4:a .eww file is generated and I opened the file using IAR software the code builds completly without erros but, I am getting the following notification during opening of file 

curiocity_2-1748856135172.png

Step 5:The code builds ok with no error so now I have tried to debug that code it will not 

Step 6:I have right click on project and tried to look the core or device but it is not detected as below (the core should be Cortex MO+and there should be Device name 

curiocity_3-1748856342426.png

My question is: Could there be an issue with the CubeMX IDE that's preventing it from detecting the STM32C071RBT6 microcontroller?

Step 7: I navigated to the ST folder in the IAR system, but I couldn't find any files related to the STM32C071RBT6. Why weren’t the files generated

curiocity_4-1748856583217.png

Observation 2:

This issue never occurred when I was using the STM32F411RE with the NUCLEO-F411 development board.

 

Could you please help me to solve the issue 

12 REPLIES 12
Andrew Neil
Super User

What EWARM version are you using?

On what host platform?

 


@curiocity wrote:

Step 4: a .eww file is generated and I opened the file using IAR software the code builds completely without errors but, I am getting the following notification during opening of file  


What do you mean by, "opening the file" here ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi Andrew,

Thanks for your reply

1.I am using IAR Embedded Workbench IDE-Arm 9.10.2 

2.Opening the file means that the generated .eww file is launched using IAR Embedded Workbench.

Thanks, but you didn't say what host - windows, linux, etc ?

 


@curiocity wrote:

2.Opening the file means that the generated .eww file is launched using IAR Embedded Workbench.


Your title says, "during debugging" - but that sounds like just initially opening the project file?

 

PS:

AndrewNeil_0-1748859635170.png

What did the log window say?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi Andrew,

I am working with Windows system 

 

Hi Andrew

Sorry for confusion,

Not during debugging I want to say during launching i.e at initial state. 

The problem itself is I am not able to do debugging because device is not detected .

IAR WB was Windows-only when I dealt with it. I'm not aware that ever changed.

Did you check what option IAR complains about ?
I suspect you are using an older version that Cube expects.

Try enabling all possible console output options in the WB, you should see an error message.


@curiocity wrote:

The problem itself is I am not able to do debugging because device is not detected .


if it's already told you on opening the Project that the Project is bad, then it's not a surprise that things don't work properly with that Project!

Are you sure that your version of IAR actually supports this chip?

You'd need to check that with IAR.

Also:

AndrewNeil_0-1748860145698.png

What did the log window say?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Are you sure that your version of IAR actually supports this chip?

ans: I'm not certain, but assuming it works with the STM32F411RE, it might also work with the STM32C071CBT6

You'd need to check that with IAR.

ans:Yes, but is this issue actually related to IAR or CubeMX?

Not able to understand from this log 

curiocity_1-1748860295517.png


@curiocity wrote:

Are you sure that your version of IAR actually supports this chip?

ans: I'm not certain


Then you need to check with IAR.

 


@curiocity wrote:

but assuming it works with the STM32F411RE, it might also work with the STM32C071CBT6


If your IAR doesn't recognise the chip, then it's not going to work!

"Non-recognized options" sounds exactly like what'd happen with a chip that's not recognised!

 


@curiocity wrote:

Not able to understand from this log 

curiocity_1-1748860295517.png


It's IAR's log - so you'd have to ask them about it.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.