2022-11-29 2:48 AM
Today my STM32CubeIDE does an update to the Version: 1.11.0 (Build: 13638_20221122_1308 (UTC) ) including the CubeMX Version: 6.7.0-RC2 (Build: 20221118-1646 (UTC))
Using the FreeRTOS Middleware the generation of the main file has a big bug. There will be the "USER CODE Header" lines instead of the FreeRTOS lines inseide the main()-function.
This happens also if I create a new empty project using the FreeRTOS middleware. It will generate the attached main-c-file. See lines 145-151.
I haven't searched where the bug comes from.
2022-11-30 4:37 AM
Having the same problem after updating STM32CubeIDE. I think this is a bug in STM32CubeMX made by ST developers.
2022-11-30 8:24 AM
I have tested a little bit with manual editing the ioc-file.
this were the lines before updating STM32CubeIDE:
MxCube.Version=6.6.1
MxDb.Version=DB.6.0.60
After the update this changed to:
MxCube.Version=6.7.0
MxDb.Version=DB.6.0.70
The code generation worked in correct way if I change to:
MxCube.Version=6.7.0
MxDb.Version=DB.6.0.61
but it does the same stupid thing if I use the new database:
MxCube.Version=6.6.1
MxDb.Version=DB.6.0.70
So it seams a problem inside the database
2022-11-30 8:59 AM
I have found it :grinning_face:
Inside the FREERTOS-STM32F4xx_Configs.xml file is a error in line 349
line 349: <RefConfigFile Description="Variable creation then launch the RTOS" Name="CREATION_V2" Template="?freertos_init_c_cmsis_v2.ftl">
line 350: <File Category="source" Condition="all" Name="rtos_obj_creat.tmp" Version="10.3.1"/>
<Argument Comment="User threads" GenericType="rtos_list" Name="Threads"/>
<Argument Comment="User queues" GenericType="rtos_list" Name="Queues"/>
<Argument Comment="User timers" GenericType="rtos_list" Name="Timers"/>
<Argument Comment="User mutexes" GenericType="rtos_list" Name="Mutexes"/>
<Argument Comment="User recursive mutexes" GenericType="rtos_list" Name="RecursiveMutexes"/>
<Argument Comment="User binary semaphores" GenericType="rtos_list" Name="BinarySemaphores"/>
<Argument Comment="User counting semaphores" GenericType="rtos_list" Name="Semaphores"/>
<Argument Comment="User events" GenericType="rtos_list" Name="Events"/> <!-- NEW FOR EVENTS -->
<Argument Comment="API in use" GenericType="simple" Name="FreeRTOS_API"/> <!-- need to distinguish CMSIS v1 and v2 -->
</RefConfigFile>
There is a question mark as first sign of the template name. Remove it and it works.
I have done a short view on other FREERTOS-STM32F configs. They are without this error.
This files comes with the STM32CubeIDE-update. So it will be overwritten if it does a new (re-)update
2022-11-30 9:04 AM
Do you work with an STM32F4xx controller? I have solved the problem :)
2022-11-30 11:45 AM
Indeed, the problem was in this sign "?" in FREERTOS-STM32F4xx_Configs.xml ....Probably someone joked in ST :face_with_tears_of_joy:. Now appeared an initialization of tasks, semaphores, mutexes after calling the osKernelInitialize() function. Thanks buddy!
2022-12-01 7:41 AM
Hello @Jens Räthe
Thank you for your contributions and for your detailed explanations,
I confirm the issue on my side, it has been reported to STM32CubeMX development team .
Internal ticket number: 140318(This is an internal tracking number and is not accessible or usable by customers).
I will keep you posted with updates.
Regards,
Ghofrane
2023-02-22 10:33 PM
It's been 3 months and a newer version of STM32CubeMX has been released, but the problem still hasn't been solved.
2023-03-07 1:15 AM
Hello @Jens Räthe
I am glad to inform you that the Internal ticket number: 140318 is fixed and integrated in the latest CubeMX version 6.8.0 .
This is the LINK for downloading it .
Thanks again for your contributions .
Ghofrane
Ghofrane.