cancel
Showing results for 
Search instead for 
Did you mean: 

Using the STM32CubeIDE, the ADC Scan Conversion Mode cannot be set to Enabled

CLee.0
Associate III

Using the STM32F303RE Nucleo, I need to put ADC1 in scan mode so I can read multiple channels. To do so, I need to set the 'Scan Conversion Mode' to 'Enabled' in the Configuration. However that is not an option in the CubeIDE. Only 'Disabled' is showing.

The only other peripheral I have is the DAC1.

How to Enable scan mode ?

1 ACCEPTED SOLUTION

Accepted Solutions
CLee.0
Associate III

OK, I actually figured it out:

You can't set it to Enabled until you first scroll down lower and choose a 'NUmber of Conversions' that is greater than 1. A bit user unintuitive... but problem solved.

View solution in original post

4 REPLIES 4
CLee.0
Associate III

PS attached is an image showing the problem...

0690X000009k4zaQAA.png

CLee.0
Associate III

OK, I actually figured it out:

You can't set it to Enabled until you first scroll down lower and choose a 'NUmber of Conversions' that is greater than 1. A bit user unintuitive... but problem solved.

GMupf.1
Associate

Thank you. That was very helpful!!

LJenn.1
Associate

Thank you, that was helpful to me too 🙂