cancel
Showing results for 
Search instead for 
Did you mean: 

USB_OTG_FS: Unselsecting "Activate_SOF" doesn't change code.

NRoth.1
Associate II

USB_OTG_FS: In one of two projects unselecting "Activate_SOF" in the .ioc environment doesn't disable its entry in the code! Error of the IDE or is there something else keeping the SOF enabled? As said, in another project it works a as expected.

0693W00000QOGqVQAX.png0693W00000QOGs1QAH.png 

4 REPLIES 4
Ghofrane GSOURI
ST Employee

Hi @NRoth.1 

I reproduced your configuration using stm32cubeMx 6.6.1 and Nucleo-F767ZI

I kept SOF disabled then I generated the code using 

stm32cube IDE and also keil I found that is working as expected 

could you please give me more details about your version of stm32cubeMx and your SOC 

0693W00000QOIL9QAP.png0693W00000QOIKpQAP.png 

Ghofrane

NRoth.1
Associate II

NUCLEO-L4A6ZG

STM32CubeIDE

Version: 1.10.1

Build: 12716_20220707_0928 (UTC)

STMicroelectronics STM32CubeMX

6.6.1.202207061420

com.st.stm32cube.common.feature.mx

NRoth.1
Associate II

As mentioned already, it is probably not easy to reproduce it, as I have a more or less exact copy of that project in which it works. (The one in which it works is setup as C++, but I doupt that has anything to do with this is the issue, but could be wrong).

Ghofrane GSOURI
ST Employee

Hi @NRoth.1

I used your stm32cubeIDE version 1.10.1 and it works just fine

0693W00000QOINeQAP.pngGhofrane