Senior
January 16, 2025
Question
ST32CubeMX 6.13.0 STM32H747 USB_DEVICE_M4 USB_OTG_FS files not included in the generated .cmake
- January 16, 2025
- 4 replies
- 843 views
STM32CubeMX 6.13.0
MCU: STM32H747
Peripheral: USB_OTG_FS
USB Class: CDC
Core: M4
FW: 1.12.1
CMake generator selected
The generated file "mx-generated.cmake" in the CM4 folder only includes the USB Class source file, but not the USB Core source files.:
../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pcd.c
../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pcd_ex.c
../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_ll_usb.c
../Common/Src/system_stm32h7xx_dualcore_boot_cm4_cm7.c
../Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Src/usbd_cdc.c
./Core/Src/sysmem.c
./Core/Src/syscalls.c
./Core/Startup/startup_stm32h747xx_CM4.s
IOC file is attached.