‎2020-01-14 1:18 AM
Upgraded STM32CubeMX from 5.4.0 to 5.5.0 and H7 firmware package to V1.6.0 and migrated.
When generating code it tells me the code is successfully generated but STM32CubeIDEproject generation have a problem.
Building the project fails:
make: *** No rule to make target 'C:/git/ELS/sbc_bootloader/CM7/Src/sys.c', needed by 'Application/User/sys.o'. Stop.
The same thing happens if I start a new project.
I'm using the STM32H745ZITx.
STM32CubeIDEproject generation have a problem, what problem?
Please fix :)
Solved! Go to Solution.
‎2020-01-15 3:02 AM
How did you​ get STM32CubeMX 5.5.0?. From complete fresh install or updating a 5.4.0 one ?.
If update could you have a try relying on your .ioc file AND complete 5.5.0 fresh install? ​
‎2020-01-15 3:19 AM
First I tried updating from CubeMX 5.4.0.
And the error came up when generating code.
Then I downgraded to 5.4.0 with a file I downloaded from the ST site.
This was last week.
Yesterday I upgraded again to 5.5.0 but this time with a file downloaded from ST site, but still the same.
‎2020-01-15 7:08 AM
​Could you please @Svenn Dahlstrom​ change the java version ? try the 1.8.0_211-b12 64bit
‎2020-01-15 7:09 AM
according to your .log file : ​Detected Java Version = 13.0.1
‎2020-01-15 7:14 AM
I will try this tomorrow :)
‎2020-01-15 7:20 AM
Yes, I updated Java SE DK to 13.0.1 from 12.0.1 yesterday before upgrading to CubeMX 5.5.0
This means that last week when I upgraded to CubeMX 5.5.0 I had Java SE DK 12.0.1 and this gave the same result.
‎2020-01-15 7:41 AM
​Okey thanks to inform me of the result obtained.
Khouloud
‎2020-01-15 11:33 PM
​Hello @Svenn Dahlstrom​ ,
Issue will be fixed in the next release,
For the moment ,please delete the binarie file under third_parties_plugins in the folder of install , and it will work.
Best Regards,
Khouloud.
‎2020-01-15 11:43 PM
Updated to java 1.8.0_211-b12 but still the same :(
java version "1.8.0_211"
Java(TM) SE Runtime Environment (build 1.8.0_211-b12)
Java HotSpot(TM) 64-Bit Server VM (build 25.211-b12, mixed mode)
‎2020-01-16 1:00 AM
Thanks @Khouloud ZEMMELI​, I deleted the folder and code generation is not having problems anymore.
But it still deletes CM7\IScr\sys.c and CM7\Inc\sys.h files :crying_face:.
Will this also be fixed in the next release?