2020-07-30 11:32 AM
With the latest version of CubeMX (Version: 6.0.0-RC5) there is a reported error with ADC configuration. I will attached the preferred configuration below. The problem is that the latest version will not let me select ADC2, see attached configuration, for 'DMA Circular Mode'. ADC1 is ok but for some reason CubeMX will no allow ADC2 to be selected as 'DMA Circular Mode'. I can only select DR or DFSDM Mode - not circular!
2020-07-31 3:53 PM
What chip?
2020-07-31 5:03 PM
2020-08-03 1:08 AM
Hello @MLane.3
Could you please share your .ioc file to check the issue.
Best regards,
Nesrine
2020-08-03 2:38 AM
Hello @MLane.3
Thanks for the feedback, issue reported to the tool development team that will plan the correction.
Best regards,
Nesrine
2020-08-03 7:28 AM
Hello @MLane.3
Sorry, It's not a bug, To activate the "DMA Circular mode" it must be configured in DMA Settings Tab.
Best regards ,
Nesrine
2020-08-04 8:56 AM
ok that fixed the problem. Why did it change though? This was fine up until I updated CubeMx.