2020-08-12 3:52 AM
Hi,
I can generate projects for keil with STMCube but when I choose FreeRTOS and keil, when I choose the compiler version to be V6, the build would fail. is there any work around this?
2020-08-12 3:54 AM
Hi @ali_dehbidi
There's an issue related to FreeRtos on 6.0.0, could you please share your ioc file ?
Thanks
Khouloud
2020-08-12 4:26 AM
2020-08-14 6:48 AM
Hello @ali_dehbidi ,
After check, Compiler V6 is not supported (it's only supported with L5).
Best Regards,
Khouloud
2020-08-15 4:05 AM
Thanks Khouloud, is there any plan for V6 support?
Regards
2022-01-17 5:17 AM
Hello @Khouloud ZEMMELI ,
I too had earlier raised a similar query, but I am unable to find it.
When will STM32CubeMX start supporting generation of MDF-ARM/Keil-compilable code which can be compiled using Compiler version 6?
As per my previous communication the only requirement is to REPLACE the FreeRTOS RVDS folder with the GCC folder.
Please help release this feature request ASAP.
Regards,
Rajeev