cancel
Showing results for 
Search instead for 
Did you mean: 

STMCubeMX generate errors in the ld script (Toolchain/IDE : Makefile)

Sylex
Associate II

Hi everybody,

I found a bug in STMCubeMX in the way it generates .ld scripts.

Context:

  • STMCubeMX  V 6.12.1 (linux)
  • EVK : NUCLEO-F446RE
  • Toolchain/IDE : Makefile
  • arm-none-eabi-gcc (GNU Arm Embedded Toolchain 10.3-2021.10) 10.3.1 20210824 (release)

Problem:

The STM32F446RE Tx_FLUSH.ld file generated by STMCubeMX contains several errors that do not allow a link to be made correctly using Makefile.

Here are the difference :

Notice:

  • the STM32F446RETx_FLASH.ld.CubeMx is the one generated by STMCubeMX
  • the STM32F446RETx_FLASH.ld is the corrected one

They are both stored in the attached zip.

diff -rup ./STM32F446RETx_FLASH.ld.CubeMx ./STM32F446RETx_FLASH.ld
--- ./STM32F446RETx_FLASH.ld.CubeMx 2024-10-06 08:43:28.775227144 +0200
+++ ./STM32F446RETx_FLASH.ld 2024-10-06 08:43:23.579187576 +0200
@@ -53,7 +53,7 @@
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
-_estack = ORIGIN() + LENGTH(); /* end of RAM */
+_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x600; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
@@ -143,7 +143,7 @@ SECTIONS

. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
- } > AT> FLASH
+ } >RAM AT> FLASH


/* Uninitialized data section */
@@ -160,7 +160,7 @@ SECTIONS
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
- } >
+ } >RAM

/* User_heap_stack section, used to check that there is enough RAM left */
._user_heap_stack :
@@ -171,7 +171,7 @@ SECTIONS
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
- } >
+ } >RAM

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Sylex 

Thanks again for sharing this with us. This behavior has been solved on the last version of the STM32CubeMX V6.13.0.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Bonjour @Sylex et bienvenue sur la communauté de ST :smiling_face_with_smiling_eyes:.

I think that this is a known regression that i have escalated for correction on the comming releases. Take a look at this post for more details.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

So, if I well understand, I must regress CubeMX  to version 6.12.0 !

Why ST is pushing release without serious test? Does STM consider us (the developers) to be the beta testers?

STTwo-32
ST Employee

Hello @Sylex 

Thanks again for sharing this with us. This behavior has been solved on the last version of the STM32CubeMX V6.13.0.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Tested and fixed, thanks