2023-04-13 03:23 AM
I want to use STM32U5 ADF in LPBAM Mode, I can't see the ADF option in the CUBE MX LPBAM design configuration. I want to use ADF in stop 2 mode with LPDMA and SRAM4 I have the ready code for ADF and LPDMA I wish to operate them in LPBAM Mode.
2023-04-13 04:46 AM
Hi @SShai.3 ,
Thank you for sharing this issue, the U5 series is one of our brand new family product and it is important to have your feedback to improve our ecosystem 🙂 .
Can you tell me which STM32U5 and CubeMX version are you using?
Best Regards,
A.MVE
2023-04-13 10:27 AM - edited 2023-11-20 08:17 AM
I am using NUCLEO-U575ZI-Q Board
STM32CUBE Mx Version: 6.8.0
I have attached the image below for your reference as you can see there is no ADF option in LPBAM Configuration.
2023-04-14 04:50 AM
Hi @SShai.3 ,
Yes the 6.8.0 is the latest CubeMX version, thank you for noticing this issue.
I will transmit it to the ecosystem team, it will be fixed on the next CubeMX release.
Thank you !
A.MVE
2023-04-14 06:04 AM
So can you assist how can i go forward?
As the ADF option is not present in CUBE MX LPBAM Config. How should I generate the startup code for ADF in LPBAM Mode?
I am not getting drivers also for the same.
2024-01-22 08:42 AM
Hello,
It's been almost a year since SShai.3 reported the issue of the missing ADF peripheral in the CubeMX LPBAM configurator. As of STM32CubeMX version 6.10.0, the ADF1 peripheral is still missing. Is there a limitation in the STM32U5 hardware that is preventing this feature from being implemented? Is there any example code that I could follow to get ADF1 working with LPDMA in STOP MODE 0 and higher?
Thank you for your time and best regards,
Rob
2024-01-23 08:14 PM
Anyone out there have information on getting the ADF peripheral working in stop mode with LPBAM? I'd really like to get this figured out. Thanks!