2023-01-13 2:20 PM
I have a nucleo-U575ZI-Q and can run the examples for the ADCs just fine. However when I try and make my own project using STM32CubeMX the code hangs at the ADC calibration. I've gone over the settings a dozen times and compared them against the example and cannot find anything different. Any insight would be helpful. Thanks
Solved! Go to Solution.
2023-01-13 2:24 PM
Ok I figure it out. But this really should be noted somewhere in the examples. This line needs run before the ADC usage. HAL_PWREx_EnableVddA(); Im sure there are other ways to setup the Voltage reference, but in the simplest case this works. In the example projects it is buried in stm32u5xx_hal_msp.c here:
void HAL_MspInit(void)
{
/* USER CODE BEGIN MspInit 0 */
/* USER CODE END MspInit 0 */
__HAL_RCC_PWR_CLK_ENABLE();
/* System interrupt init*/
/* USER CODE BEGIN MspInit 1 */
HAL_PWREx_EnableVddA();
HAL_PWREx_EnableVddIO2();
/* USER CODE END MspInit 1 */
}CubeMX doesnt seem to generate this, it looks like whoever made the example stashed those lines there.
2023-01-13 2:24 PM
Ok I figure it out. But this really should be noted somewhere in the examples. This line needs run before the ADC usage. HAL_PWREx_EnableVddA(); Im sure there are other ways to setup the Voltage reference, but in the simplest case this works. In the example projects it is buried in stm32u5xx_hal_msp.c here:
void HAL_MspInit(void)
{
/* USER CODE BEGIN MspInit 0 */
/* USER CODE END MspInit 0 */
__HAL_RCC_PWR_CLK_ENABLE();
/* System interrupt init*/
/* USER CODE BEGIN MspInit 1 */
HAL_PWREx_EnableVddA();
HAL_PWREx_EnableVddIO2();
/* USER CODE END MspInit 1 */
}CubeMX doesnt seem to generate this, it looks like whoever made the example stashed those lines there.
2023-01-19 2:05 AM
Hi @ASimo.3 ,
The sequence to be applied in order to enable analog peripherals is described in page 371 of RM0456 (paragraph: Peripheral voltage monitoring (PVM)).
So, in your case, only HAL_PWREx_EnableVddA() is required unless you need to use one of the pins GPIOG[15:2].
I confirm that this needs to be generated by STM32CubeMX, so thanks for bringing this issue to our attention. I reported issue internally.
Internal ticket number: 143303 (This is an internal tracking number and is not accessible or usable by customers).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.