cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753 change frequency in the older version to 480MHz

kulfi27
Associate II

Hello everyone, at the beginning of this year I bought a microcontroller, it was a version with 400MHz clocking, at the moment CubeMX allows you to change the frequency to 480MHz, can I change it, will everything work properly. Best Regards

3 REPLIES 3
PMath.4
Senior III

I've got 400MHz spec H743's running at 540MHz with no issue including running FMC, LTDC and USB peripherals

Ozone
Lead III

The maximal core clock speed specified in the datasheet is guaranteed for the whole temerature range, especially the maximum temperature.

Expect fails (crashes) at higher temerature with overclocked devices.

kulfi27
Associate II

Thank you for the quick reply, I will take this into account.