2019-11-29 1:32 AM
Hello everyone, at the beginning of this year I bought a microcontroller, it was a version with 400MHz clocking, at the moment CubeMX allows you to change the frequency to 480MHz, can I change it, will everything work properly. Best Regards
2019-11-29 1:45 AM
I've got 400MHz spec H743's running at 540MHz with no issue including running FMC, LTDC and USB peripherals
2019-11-29 2:40 AM
The maximal core clock speed specified in the datasheet is guaranteed for the whole temerature range, especially the maximum temperature.
Expect fails (crashes) at higher temerature with overclocked devices.
2019-11-29 5:52 AM
Thank you for the quick reply, I will take this into account.