2021-09-08 01:05 PM
In ST Cube IDE 1.6.0 project, Cube MX view - > vrefbuf is missing from syscfg page
Solved! Go to Solution.
2021-09-08 02:43 PM
The STM32G491KE doesn't have a VREF+ pin. It's bonded internally to VDDA. Enabling the voltage buffer would mean it would need to fight with VDDA, clearly not a workable scenario.
From the datasheet:
The VREF+ pin is double-bonded with VDDA on some packages. In these packages the internal voltage reference buffer is not available.
2021-09-08 01:48 PM
It's there for me. Share your IOC file if able and/or screenshot. CubeIDE v1.7.0 is latest.
2021-09-08 01:59 PM
2021-09-08 02:43 PM
The STM32G491KE doesn't have a VREF+ pin. It's bonded internally to VDDA. Enabling the voltage buffer would mean it would need to fight with VDDA, clearly not a workable scenario.
From the datasheet:
The VREF+ pin is double-bonded with VDDA on some packages. In these packages the internal voltage reference buffer is not available.