2022-02-27 9:05 PM
hey there,
I have a STM32G030C8t6 which I wish to configure. in CubeMX when I focus on PA11 or PA12, I can see a bracket where this is mentioned:
PA11[PA9]
PA12[PA10]
what does it mean? does it mean they are somehow connected or related?
can anyone explain it?
thanks in advance
Solved! Go to Solution.
2022-02-27 10:10 PM
See DS12991 datasheet: Table 12 Foot note 4: "Pins PA9 and PA10 can be remapped in place of pins PA11 and PA12 (default mapping), using SYSCFG_CFGR1 register."
Check the other foot notes to avoid surprises.
hth
KnarfB
2022-02-27 10:10 PM
See DS12991 datasheet: Table 12 Foot note 4: "Pins PA9 and PA10 can be remapped in place of pins PA11 and PA12 (default mapping), using SYSCFG_CFGR1 register."
Check the other foot notes to avoid surprises.
hth
KnarfB
2022-02-28 12:23 AM
so if I set SYSCFG_CFGR1 register in my code, I can use those Pins alternatively, right?
and the whole process should be done without CubeMx right?
2022-02-28 12:41 AM
Correct
hth
KnarfB