2019-05-03 7:59 AM
Hello,
I test the CDC with my STM32F407VgTx in an up-to-date environment:
Windows 10 / STM32CubeMx v5.20 / SW4STM32 / System WorkBench for STM32/ST-LINK V2
The VCP v 1.50 driver for windows 10 has been installed normally and declared active.
The source of the CDC program used is:
\ STM32Cube_FW_F4_V1.24.0 \ STM32Cube_FW_F4_V1.24.0 \ Middleware \ ST \ STM32_USB_Device_Library \ Class \ CDC
When running the program, when init the USB, I get Windows Error 43.
Unknown USB Device (descriptor request failure).
Can you help me solve this problem?
In advance thank you
Robert
2019-05-10 1:18 AM
Hello Christian,
The retrogradation of the 6 files did not solve the problem.
My anomaly has causes different from those you hads
Thanks
Robert
2019-05-10 1:32 AM
2019-05-10 2:44 AM
The picture you've posted 2 days ago shows a problem with USB clock. Have you resolved it? Does the board have external oscillator for HSE?
-- pa
2019-05-10 4:00 AM
Hello,
Sorry to have mixed HSE / HSI in the text 2 days ago.
My card has an external crystal of 26 Mhz / HSE
I'm doing my tests in this extern crystal config
I had been told that the CDC was working in 16 Mhz / HSI but when I saw that there were clock config problems I did not try.
That said if there was a solution to work with the USB without extern crystal outside I would be a taker.
Rob
2019-05-10 4:17 AM
2019-05-11 2:29 PM
> if there was a solution to work with the USB without extern crystal outside I would be a taker.
Some MCUs with device-only controller (F072 for example) can derive the USB clock from host, using SOF.
They can work without external crystal. I don't know whether OTG can do this, even in device mode.
-- pa
2019-05-13 11:09 AM
Hello,
After having done, with the community that was interested in this problem, all the investigations that seemed interesting to us,
the problem I described is not solved .
My last investigations with DBG_Trace (present in the project) allowed me to see that the interrupts resulting from a request of the driver (OTG_FS_IRQHandler > HAL_PCD_IRQHandler (& hpcd_USB_OTG_FS) are active and processed but I could not delve deeper to locate the problem ...
The VCP driver for Windows10 does not receive (in 3ms I believe) correct information in descriptor (for him) and reports it in the program manager of Windows 10.
The same thing happens under Windows 7 professionnal.
It should be noted that this driver works without error with several other VCP applications found on the net that I tested on my DIYMORE card.
We can think that the problem lies in the libraries of version 1.24 / 1.24.1 or in the projet generated by CubeMX .
I am attaching my complete project.
Hoping to have a solution as soon as possible ....
At advance thanks.
Regards.
Robert
2019-05-14 11:54 AM
I think I'm having the same problem (but with an L4 and F7 board). I've got debug output on another thread: https://community.st.com/s/question/0D50X0000Ap1YIzSQM/do-the-virtual-com-port-drivers-work-with-windows-7
Please take a look and see if this is similar to your issue.
When I run it on a Windows 7 system, I get the USB error 10. Window Server 2012 systems shows USB error 43.
The issue I'm seeing has been fixed. It was an unaligned memory access in USB_WritePacket.
2019-05-14 11:10 PM
Hello,
Thank you for your information.
My error code is different from yours : 43 in Windows 7 and 10 .
I still modified USB_Write Packet (...) but the problem has not been solved.
2019-05-29 9:05 AM
Hello,
Same problem with last version (5.2.1) of STM32CubeMX.
Sorry.
Robert.