2022-03-11 08:06 AM
2022-03-11 08:31 AM
in the .ioc view, Project Manager tab, Advanced Settings is a table Generated Function Calls. If you select a line, you may change the init order by pressing one of the cryptic little blue icons in the upper left corner. Some settings can be moved, others not. Good luck
KnarfB
2022-03-11 08:41 AM
Thanks for your quick reply.
That basically seems to be the right place to change that. Unfortunately in my case these 2 buttons are greyed out.
Maybe not generating a function call by MX and calling the function in the user code section helps.
2022-03-11 08:54 AM
In similar cases, I had put a copy of the DMA init call in a user block ahead and left the generated code as is.
KnarfB
PS: That's an evergreen: https://community.st.com/s/feed/0D53W000019c1TDSAY
2022-03-11 09:01 AM
Yes found that one too :D
But since this is known for more than two years now and there is no way to send a classic bug report thought I'll "push" this topic at least agein.
Actually I hope that ST might react someday to this and fix it...