2024-03-14 12:40 AM
I have installed STM32CubeMX version 6.10.0 in Ubuntu 22.04 (through Windows Subsystem for Linux 2), but when I start it and click "INSTALL/REMOVE" to install the X-CUBE-AI extension, I get the following error message and nothing more happens:
[ERROR] CheckServerUpdateThread:123 - Unexpected exception CheckServer ThreadCannot invoke "com.teamdev.jxbrowser.browser.Browser.mainFrame()" because "this.browser" is null
I have tried manually installing Chromium and restarted the system after that, but I still get the same error.
How can I get the installation procedure to work?
2024-03-14 03:59 AM
Hello @magnus_lindhe ,
First let me thank you for posting.
This issue is under investigation, and I will get back to you as soon as possible.
Thanks.
Mahmoud.
2024-03-27 02:19 AM
Hello @magnus_lindhe ,
The issue was not reproduced. The installation of X-Cube-AI extension was successful using STM32CubeMX 6.10.0 and Ubuntu 22.04.
I suggest that you download the package from this link X-CUBE-AI - AI expansion pack for STM32CubeMX - STMicroelectronics and load it manually.
Thanks.
Mahmoud.