cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX on Ubuntu 22.04: Cannot launch browser to install X-CUBE-AI

magnus_lindhe
Associate II

I have installed STM32CubeMX version 6.10.0 in Ubuntu 22.04 (through Windows Subsystem for Linux 2), but when I start it and click "INSTALL/REMOVE" to install the X-CUBE-AI extension, I get the following error message and nothing more happens:

 

[ERROR] CheckServerUpdateThread:123 - Unexpected exception CheckServer ThreadCannot invoke "com.teamdev.jxbrowser.browser.Browser.mainFrame()" because "this.browser" is null

 

 

I have tried manually installing Chromium and restarted the system after that, but I still get the same error.

How can I get the installation procedure to work?

 

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @magnus_lindhe  ,

First let me thank you for posting.

This issue is under investigation, and I will get back to you as soon as possible.

Thanks.

Mahmoud.

Mahmoud Ben Romdhane
ST Employee

Hello @magnus_lindhe ,

The issue was not reproduced. The installation of X-Cube-AI extension was successful using STM32CubeMX 6.10.0 and Ubuntu 22.04.

I suggest that you download the package from this link X-CUBE-AI - AI expansion pack for STM32CubeMX - STMicroelectronics and load it manually.

Thanks.

Mahmoud.