2020-02-10 5:17 AM
Up till now (v1.6.0) there is no support for PTP in MAC Ethernet driver. WHen will it be added?
2020-02-10 3:18 PM
Better worry about the fact that H7 driver is not working at all...
As for PTP - it's a pretty simple (part of) peripheral. It's hard to even imagine what a PTP "driver" should do. Write few integer values into registers through one line long functions like in LL "drivers"?
2020-02-11 2:37 AM
Pretty simple, that's why I wander why is it not realized yet?
Up till now I was working on F7 series, and now our company desided to move to H7.
Not working at all? What I see is that RX and TX frames are getting transferred well. LwIP is going to be the next step to run.
2020-02-11 3:00 AM