2024-10-01 10:46 AM
Hello everyone,
I’m currently working on configuring the memory mapping for the STM32G431KB3U and ran into a bit of a roadblock. I was expecting to find a memory management section under the Tools tab in STM32CubeMX, but I didn’t see anything there.
Additionally, I’ve searched through the documentation for the STM32G431KB3U, but I couldn’t find any information regarding whether this feature is available or not.
Could anyone clarify if memory management configuration is supported in STM32CubeMX for the STM32G431KB3U? Any insights or guidance would be greatly appreciated!
Thank you!
Solved! Go to Solution.
2024-10-01 12:20 PM
Hello @gwe and welcome to the ST Community :smiling_face_with_smiling_eyes:.
As you can see on the RN0094, the memory management tool has been implemented for the first time on the V6.9.0 of the CubeMX for only STM32H5 and STM32U5. After that they added the STM32WB and STM32WBA on the V6.10.0, the STM32H7R/S and STM32H533/523 on the V6.11.0 and theSTM32H7 Single core together with the STM32WB0 for the last version 6.12.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-01 12:20 PM
Hello @gwe and welcome to the ST Community :smiling_face_with_smiling_eyes:.
As you can see on the RN0094, the memory management tool has been implemented for the first time on the V6.9.0 of the CubeMX for only STM32H5 and STM32U5. After that they added the STM32WB and STM32WBA on the V6.10.0, the STM32H7R/S and STM32H533/523 on the V6.11.0 and theSTM32H7 Single core together with the STM32WB0 for the last version 6.12.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.