2024-08-26 08:35 PM - last edited on 2024-08-30 02:30 AM by SofLit
Hi. I am using NUCLE-F439ZI board
STM32CubeIDE Version: 1.16.0
Build: 21983_20240628_1741 (UTC)
Lately I am experiencing problem, when I make changes in .IOC file and save and generate code
it is messing my main.c file. It is copying big portion of main.c lines and adding them again in main.c file.
It is impossible to continue working. Is this a setting problem or a bug in the software?
Please help.
Thank you.
Rasem
2024-08-27 05:44 AM
Are you modifying the USER CODE lines? What lines is it copying/adding? Your code should only be put within a USER CODE block.
Include your main.c file here.
2024-08-27 06:58 AM
Hello,
Are you putting your custom code between:
/* USER CODE BEGIN XXX */
<Your custom code>
/* USER CODE END XXX */
2024-08-27 09:12 AM
HI SofLit,
Thanks for the reply.
Yes, all codes are between the user specified locations. The problem happens when I copy and paste some code from
another project, and then I make changes in .IOC file, Save and generate code.
Now, I am trying now to Build the project every time I paste a new code, and before I make changes in .IOC and before
Generating code. It seems to be working without problem.
This is my assumption of the problem, I hope it will solve future problems.
Rasem
2024-08-27 09:18 AM
Could you please describe the exact operation you are doing?
Could you please share the exact code you are copying/pasting in the generated code and where? Is the code you are copying contains /* USER CODE BEGIN XXX */ and /* USER CODE END XXX */ ?
2024-08-27 03:03 PM
2024-08-27 03:17 PM
But you didn't answer these questions:
Could you please describe the exact operation you did?
Could you please share the exact code you are copying/pasting in the generated code and where?
We need to know which code was generated and which user code you paste and were?
For that, we need from you to:
1- Provide the original main.c generated code
2- Provide the user code and where you paste it? at which lines
3- Attach the .ioc file to reproduce the behavior.
Thank you.