2022-07-25 01:09 PM
@Piranha pointed me to a fault in the configuration of the RCC in an example related to LW-IP.
I have the impression that this fault is also created when STM32cubeIDE creates the default settings for the STM32H735G -DK Discovery kit.
The manual RM0468 is clear:
The schematic of the STM32H735G-DK kit:
X2 is a crystal, X1 is an oscillator:
BOM says the same:
But STM32CubeIDE initialized as per the board:
And should be: (IMHO)
My question: Is my analysis correct or did I overlook something?