cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE appears to be missing DMA TIM15_TRIG connection option for STM32G431KB

etheory
Senior II

I want to add a TIM15_TRIG connection (is this the same as TRGO?) to a DMA transfer request.

When trying to do this via STM32CubeIDE "Version: 1.11.2 Build: 14494_20230119_0724 (UTC)" I get the following options:0693W00000aIaI1QAK.pngi.e. no option to select TIM15_TRIG, which appears to be shown to be supported in RM0440:

0693W00000aIaILQA0.pngCould this please be added to the interface so I can set it please?

And if it cannot be set in the STM32G431KB MCU, could you please update the documentation to reflect this fact please?

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions

> (is this the same as TRGO?)

No, it's (roughly) the same as TRGI.

JW

View solution in original post

2 REPLIES 2

> (is this the same as TRGO?)

No, it's (roughly) the same as TRGI.

JW

Regardless the interface is missing options that the datasheet suggests are possible.​