2017-04-06 11:05 PM
Hello,
im using the STM32F407 DIS with CubeMX to generate a USB CDC device.
All works fine but if i unplug the STM32f407 and then plug in, Windows 10 didnt detect the driver(just unknown USB-Device)
i have to reset the STM and then Windows detect the driver.
What can i do to use the STM32 with plug and play?
i use VCP 1.4
#vcp-stm32f4 #cubemx-f42017-04-07 5:30 PM
whats wrong with plug and pray ? thanks to Bill, we have got use to Re-Booting...
if you look below on this page, it has related content.
you can search the previously answered questions, there is a goldmine of information here.