2023-09-28 3:21 PM - edited 2023-10-23 2:29 AM
Hello.
To generate a multiplatform code I defined a SW architecture and packaging as follow :
Build system :
At first sight the APP would be a complete application and the LLD a library providing only the HAL calls. That would mean that the APP hosts :
I am not sure the HAL could work with independently defined interrupt handler so I let those be part of LLD except the linker script (present but not used).
The LLD package contains :
Issue to create the HAL as library : it needs to be configured as a full binary. The workaround was to let it as is for project generation, and then in the project setting change the artefact to build as static library.
When launching, the sw hangs at startup, with an "unexpected interrupt".
I can bet it is the systick since the value is always 0 before the crash :
Also I called in the app code HAL_SuspendTick, and the crash does not happen anymore.
I’ve check where is put the vector table in the map :
.isr_vector 0x0000000008000000 0xbc
0x0000000008000000 . = ALIGN (0x4)
*(.isr_vector)
.isr_vector 0x0000000008000000 0xbc CMakeFiles/test_g0b1re_app.dir/Startup/startup_stm32g0b1retx.s.obj
0x0000000008000000 g_pfnVectors
0x00000000080000bc . = ALIGN (0x4)
I have checked where is put the systick handler :
0x0000000008000690 SysTick_Handler
But in fact in the list file I don’t find it at this address but the default handler :
08000690 <ADC_COMP_IRQHandler>:
* @retval : None
*/
.section .text.Default_Handler,"ax",%progbits
Default_Handler:
Infinite_Loop:
b Infinite_Loop
8000690: e7fe b.n 8000690 <ADC_COMP_IRQHandler>
So during linkink process the Systick_Handler is replaced by the default handler, but why ?
I checked the :
I also checked the generated command lines to build :
arm-none-eabi-gcc -o "test_g0b1re_app_cdt.elf" @"objects.list" -Wl,--start-group -ltest_stm32_g0b1re_executable -Wl,--end-group -mcpu=cortex-m0plus -T"/home/ /dev/test_g0b1re_app_cdt/STM32G0B1RETX_FLASH.ld" --specs=nosys.specs -Wl,-Map="test_g0b1re_app_cdt.map" -Wl,--gc-sections -static -L"/home/test_stm32_g0b1re_executable/Debug" --specs=nano.specs -mfloat-abi=soft -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
I Tried to :
Always same result : falls in default handler.
Now it works with the followings :
So again how can the Systick_Handler be removed during compilation ? How can I avoid that ?
EDIT :
So thanks to chat-GPT I could resolve this by adding the linker option : -Wl,--whole-archive -ltest_stm32_g0b1re_executable -Wl,--no-whole-archive
I see a small increase in code size in flash, probable for the function added. I assume that with -gc-sections options, the linker will remove the not used functions. I shall check this with a complex project.
Solved! Go to Solution.
2023-10-04 9:45 AM - edited 2023-10-06 8:14 AM
Good links indeed !
Actually I like this mechanism to prevent not managed IRQ detection. Where would it land otherwise ?
I'm not sure what is doing ,--whole-archive : scan the whole archive, or embbed it completely.
If the latter is the right behavior, does --gc-sections compensate ? YES actually.
For me then the right thing to do is using --whole-archive to scan all archive with --gc-sections to remove unused code.
2023-09-29 6:16 AM
Resolving strong/weak definitions within the gcc linker for libraries is problematic. Jump down the rabbit hole if you want, but commenting out the weak definition is probably the best solution here.
https://stackoverflow.com/questions/23079997/override-weak-symbols-in-static-library
Lots of others...
2023-09-29 6:36 AM
Looks spooky... another breaking change in the latest GNU compiler & linker? The non-weak functions (of the main app) go before the lib on the link command line. Or not? Can you show the linker command line?
2023-10-04 9:37 AM
Hello.
The generated command line is already in the post.
For information I also copy the command line generated with cmake, results are equals to cdt build :
/usr/bin/cmake -E cmake_link_script CMakeFiles/test_g0b1re_app.dir/link.txt --verbose=1
arm-none-eabi-gcc -mcpu=Cortex-M0plus -std=gnu11 --specs=nano.specs -mthumb -Wall -Werror -g -T../STM32G0B1RETX_FLASH.ld --specs=nosys.specs -Wl,-Map=test.map -Wl,--gc-sections -static -Wl,--start-group -lc -lm -Wl,--end-group CMakeFiles/test_g0b1re_app.dir/Startup/startup_stm32g0b1retx.s.obj CMakeFiles/test_g0b1re_app.dir/Sources/app_main.c.obj CMakeFiles/test_g0b1re_app.dir/Sources/syscalls.c.obj CMakeFiles/test_g0b1re_app.dir/Sources/sysmem.c.obj -o test_g0b1re_app.elf -L/home/workspace/test_g0b1re_app/../test_stm32_g0b1re_executable/Debug -ltest_stm32_g0b1re_executable
arm-none-eabi-gcc -o "test_g0b1re_app_cdt.elf" @"objects.list" -mcpu=cortex-m0plus -T"/home/nautilus/dev/MCB-RT_Prod/test_g0b1re_app_cdt/STM32G0B1RETX_FLASH.ld" --specs=nosys.specs -Wl,-Map="test_g0b1re_app_cdt.map" -Wl,--gc-sections -static -L"/home/dev/test_stm32_g0b1re_executable/Debug" --specs=nano.specs -mfloat-abi=soft -mthumb -Wl,--start-group -lc -lm -Wl,--end-group -Wl,--whole-archive -ltest_stm32_g0b1re_executable -Wl,--no-whole-archive
2023-10-04 9:45 AM - edited 2023-10-06 8:14 AM
Good links indeed !
Actually I like this mechanism to prevent not managed IRQ detection. Where would it land otherwise ?
I'm not sure what is doing ,--whole-archive : scan the whole archive, or embbed it completely.
If the latter is the right behavior, does --gc-sections compensate ? YES actually.
For me then the right thing to do is using --whole-archive to scan all archive with --gc-sections to remove unused code.