2019-10-26 5:17 PM
I am working on a STM32f030.
I need to convert 2 channels of ADC, and decided to use DMA.
After reading the "HAL ADC Generic Driver" - UM1785 section, I got the idea that I don't have to use the "HAL_ADC_MspInit ()" function.
However, nothing works until I call this function again.
The following code is only for debugging and demonstrating the idea. Don't mind the rawness of it.
Do not work:
volatile uint16_t ADC_DMA[2] =
{ 0 };
uint32_t timeout_ms;
while (1)
{
timeout_ms = HAL_GetTick() + 50;
adc_conv_done_flag = 0;
HAL_ADC_Start_DMA(&hadc, (uint32_t*) ADC_DMA, 2);
while (adc_conv_done_flag == 0)
{
if (HAL_GetTick() > timeout_ms)
break;
}
HAL_ADC_Stop(&hadc);
HAL_Delay(500);
}
It works:
volatile uint16_t ADC_DMA[2] =
{ 0 };
uint32_t timeout_ms;
HAL_ADC_MspInit(&hadc);
while (1)
{
timeout_ms = HAL_GetTick() + 50;
adc_conv_done_flag = 0;
HAL_ADC_Start_DMA(&hadc, (uint32_t*) ADC_DMA, 2);
while (adc_conv_done_flag == 0)
{
if (HAL_GetTick() > timeout_ms)
break;
}
HAL_ADC_Stop(&hadc);
HAL_Delay(500);
}
PS: adc_conv_done_flag is set on "HAL_ADC_ConvCpltCallback()" function.
Something here is not working as it should ... I've already lost a few hours following the ST documentation.
Solved! Go to Solution.
2022-12-27 2:46 AM
I'm facing CubeIDE still not allowing the MCU to be changed on projects without hacking the cproject and .ioc files, and the dual ADC regular mode still generating Irqs for both ADCs, and no reply from your colleagues about this issue
2022-12-27 3:59 AM
Hi @Robmar ,
1- Please, let us keep only one topic per thread.
2- May you share links to discussions where our support is still required? Very long discussions without describing exactly the issue are generally misleading.
3- As already said privately, we cannot ensure one to one support via Community; this is not the target here. For dedicated support, you need to contact your FAE.
Thanks for your understanding.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.